web counter

Electronic components in a smart watch

Published: 15 May 2023 | Last Updated: 15 May 202310953
One of the consumer goods categories with the greatest rate of growth is wearables, which heavily rely on electronics miniaturization. Customers are becoming more and more reliant on smartphones and smartwatches that have a wide range of services, including those that measure their daily steps, display health metrics, schedule appointments, send emails, and more.

1. Introduction


One of the consumer goods categories with the greatest rate of growth is wearables, which heavily rely on electronics miniaturization. Customers are becoming more and more reliant on smartphones and smartwatches that have a wide range of services, including those that measure their daily steps, display health metrics, schedule appointments, send emails, and more. Finally, there are earphones that produce high-quality stereo sound without cords. Smart glasses with built-in cameras, video, and augmented reality capabilities would soon be available on the market. All of these devices have one thing in common: they are miracles made possible by miniaturization and incredible advancements in design and manufacturing. We need novel strategies to get there because this goes beyond the size reductions enabled by semiconductor device shrinkage. 'SiP', or system in packaging technology, is one of the most effective of the strategies being introduced. Simply said, SiP technology is a sealed package that contains all of an electronic subsystem's active and passive parts, as well as the necessary interconnections. One benefit is that high operating speeds can be attained because the interconnections are brief. Components can also be stacked within the packaging to make the best use of available space, which is essential for wearable electronics. The package is also protected from the outside environment because it is totally sealed. True Wireless Stereo, which is included in the current generation of smart earbuds, is a superb illustration of the SiP technique being successfully applied in wearable technology. Electronic subassembly miniaturization frees up space, allowing designers to fit larger and more powerful batteries without increasing the size of a gadget.

2. Components of A Smartwatch

 

A smartwatch is made up of numerous tiny components, the most obvious of which are the watch body and the strap. There is a wide variety of materials that can be used to make watch straps. The body of the watch is made up of several electronic parts such as sensors, semiconductors, batteries, touch screens, and displays. Smartwatches, in contrast to conventional electronic wristwatches, rely heavily on the array of electronic components built into the device. Smartwatches may be compact, but they pack a lot of useful features onto a single device. Radiofrequency boards, Bluetooth boards, Wi-Fi boards, boards for managing electricity, and other sensors or chips are all examples of modules.

This article mainly lists the 7 most used sensor types in smartwatches currently on the market, namely:


ü Accelerometer

ü Heart Rate Monitor

ü GPS

ü Gyroscope

ü Screen

ü Processor


1. Accelerometer

 

In general terms, an accelerometer can tell if the user is in motion since it measures acceleration, or the rate at which an object's velocity changes. Therefore, it is the sensor of choice for all smartwatches. For example, all Starmax wristwatch series are equipped with accelerometers to measure users’ movements, such as S5, S90 (kids watch), and GTS2.


Accelerometer Apps for iPhone .jpg

Figure 1: Accelerometer Apps for iPhone

 

2. Heart Rate Monitor


A heart rate monitor (HRM), sometimes known as a heart rate sensor, is a device used to monitor and record a person's heart rate and pulse. Nowadays, most smartwatches include this type of sensor incorporated to enable heart rate detection abilities. Starmax included a heart rate sensor in the GTS4 that detects blood flow via photoplethysmography (PPG) to provide accurate readings of the wearer's pulse and heart rate. The heart is a crucial organ that oversees blood flow in the human body. A healthy circulation will deliver the right quantity of blood to all organ parts at an acceptable speed. Thus, alterations in blood volume are strongly linked to pulse rate. Most smartwatches incorporate heart rate sensors that work on this concept to assess the wearer's pulse and heart rate by monitoring blood flow at the wrist.PPG (photoplethysmography) is the most extensively utilized method for heart-rate detection. It is a non-invasive monitoring method that uses optical means to monitor changes in hemoglobin volume. All Starmax smartwatch models, including the S90 (Starmax kids wearable), GTS1, GTS2, and S50, include PPG heart rate sensors. From the spectroscopy context, red and green are opposite colors, so in principle, red plasma will absorb green light. Because of its ability to detect heart rate and pulse by monitoring the variation in the strength of reflected green light, the PPG heart rate monitor is an important sensor.

3. Gyroscope

 

Gyroscopes and accelerometers are two kinds of sensors used to gauge the acceleration of an object, but they work similarly. Gyroscopes are used primarily for recording the angle of an object to record its velocity of rotation and direction changes. For a more precise orientation of objects, some smartwatch manufacturers use a combination of accelerometers and gyroscopes for triangulation. Gyroscopes and accelerometers are two types of devices used to gauge the velocity of an item, but they work differently. Gyroscopes are used primarily to track the angle of a thing in order to capture its angular velocity as well as orientation changes. For a more precise orientation of objects, some smartwatch manufacturers use a combination of accelerometers and gyroscopes for triangulation.


4. GPS


Global Positioning System (GPS), another popular function in high-end smartwatches, uses signals from satellites to identify a device’s precise position and follow its movement over time. As a result, it makes step counts more precise. Additionally, it can provide a more thorough picture of your daily activity levels (for instance, by outlining the best routes for running and cycling). The price is rather high, however, because GPS smartwatches have relatively strict signal reception requirements. For GPS smartwatches, real-time location also equals shorter battery life.


Smartwatch with GPS+LBS Tracker.jpg

Figure 2:Smartwatch with GPS+LBS Tracker


5. Screen 


The primary means of presentation and input is a smartwatch display. The screen is split into an inductive touch panel on one side and a smart display on the other. OLED, E-ink, conventional LCD, and Sharp storage LCD are the four most common display technologies for smartwatches. Some manufacturers have even debuted "soft screen" smartwatches that utilize microelectromechanical system (MEMS) technology. LED and E-ink screens are currently the most popular due to their low power requirements.


6. Processor 


The majority of licensed engines in timepieces are made by Advanced RISC Machines (ARM). Even if there are other options available. The application processors in smartwatches consume less power than those in computers. They are also more space-efficient on the board. In today's market, consumers may choose from a wide variety of high-quality chipset applications. Find out what processor is optimal for your smartwatch by doing some research or consulting a professional. The new silicon not only permits smaller hardware with larger batteries, but it also features an independent inexpensive display processor (Cortex-M55) that enables Always-on-display capabilities with minimum drain on battery life. The GPS (GNSS) L1 and a 4G LTE Cat.4 modem are also included for monitoring motion.


7. Wireless Chipset 


This is yet another feature that can't be missing from a smartwatch. The majority of the information relayed by these watches is accomplished through wireless capabilities including GPS, WiFi, Bluetooth, and NFC. Since smartwatches are so compact, most manufacturers choose chipsets that already contain these features. Therefore, they require components with a small footprint. In addition to chipset size, power consumption is a crucial factor to think about. The synchronization feature found in most modern smartwatches requires the permanent activation of a chipset. As a result, this factor's power regulation must be given serious thought.


3. Conclusion:


In conclusion, smartwatches are potent tools for effectively monitoring our physical well-being through various sensors, including the 7 sensors mentioned in this article. Furthermore, smartwatch technology will continue to evolve with advances in sensors, semiconductors, and other components. By effectively combining these various smartwatch sensors and parts, we can open up a world of infinite possibilities with our smartwatch devices. With the combination of innovation and practicality in smartwatch design, smartwatches will significantly impact the lifestyle in the coming years. The popularity of smartwatches has exploded in the past few years, but it will only continue to soar in the years to come. Even if this has a brighter future in the electronics business, it will never be able to compete with the huge market for smartphones and tablets. Analysts believe that the wearables sector is full of hype, with optimistic predictions that may not pan out. As a result, it still can't compete with smartphone usage, as many of the features are the same. Despite this, consumers are prepared to spend money on these wristwatches for purely aesthetic reasons.


4. References :

[1] G. Hindricks, T. Potpara, N. Dagres, E. Arbelo, J.J. Bax, C. Blomström-Lundqvist

Eur. Heart J. (2020)

[2] Letter to the Editor—Lifesaving therapy inhibition by phones containing magnets Heart Rhythm., (2021)

[3] Magnetic interference on cardiac implantable electronic devices from Apple iPhone Magsafe technology 10 (2021)


UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Related Articles

  • Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Saumitra Jagdale15 March 20242928

    For a long era, silicon has stood out as the primary material for fabricating electronic devices due to its affordability, moderate efficiency, and performance capabilities. Despite its widespread use, silicon faces several limitations that render it unsuitable for applications involving high power and elevated temperatures. As technological advancements continue and the industry demands enhanced efficiency from devices, these limitations become increasingly vivid. In the quest for electronic devices that are more potent, efficient, and compact, wide bandgap materials are emerging as a dominant player. Their superiority over silicon in crucial aspects such as efficiency, higher junction temperatures, power density, thinner drift regions, and faster switching speeds positions them as the preferred materials for the future of power electronics.

    Read More
  • Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    UTMEL29 August 20255726

    This comprehensive guide explores FPGAs as powerful AI accelerators that offer distinct advantages over traditional GPUs and CPUs. FPGAs provide reconfigurable hardware that can be customized for specific AI workloads, delivering superior energy efficiency, ultra-low latency, and deterministic performance—particularly valuable for edge AI applications. While GPUs excel at parallel processing for training, FPGAs shine in inference tasks through their adaptability and power optimization. The document covers practical implementation challenges, including development complexity and resource constraints, while highlighting solutions like High-Level Synthesis tools and vendor-specific AI development suites from Intel and AMD/Xilinx. Real-world applications span telecommunications, healthcare, autonomous vehicles, and financial services, demonstrating FPGAs' versatility in mission-critical systems requiring real-time processing and minimal power consumption.

    Read More
  • The 2026 Engineer’s Guide: Choosing the Right MCU for Your Next IoT & New Energy Project
    The 2026 Engineer’s Guide: Choosing the Right MCU for Your Next IoT & New Energy Project
    UTMEL30 April 20262139

    A comprehensive comparison of 2026's leading MCUs from ST, NXP, and Microchip across power efficiency, processing performance, connectivity, and ecosystems to help engineers select the optimal chip for next-gen IoT and new energy projects.

    Read More
  • AI Server Components: Engineering Next-Gen Data Center Hardware for 100kW Racks
    AI Server Components: Engineering Next-Gen Data Center Hardware for 100kW Racks
    UTMEL15 May 20261128

    The transition from traditional enterprise IT to AI-driven workloads has rendered legacy data center hardware obsolete, forcing infrastructure planners to re-engineer server components for extreme thermal environments.

    Read More
  • The Practical Engineer’s Guide to the NE555N Timer: Pinout, Setup, and Troubleshooting
    The Practical Engineer’s Guide to the NE555N Timer: Pinout, Setup, and Troubleshooting
    UTMEL29 May 2026981

    This comprehensive guide explores the NE555N timer, detailing its 8-pin layout, internal architecture, and key datasheet specifications. It compares the bipolar IC to CMOS variants and details setup configurations for astable, monostable, and bistable modes. Additionally, the guide offers practical troubleshooting advice to prevent common breadboard failures, such as floating reset pins and electrical noise issues.

    Read More

Subscribe to Utmel !

Featured Parts More